Define whether User Types can Disable Alarms Independently

Geo SCADA Expert has an Independent feature that is designed to stop potential conflicts relating to the Disable Alarms and Enable Alarms actions.

When Independent is enabled, each of the User Types (User, Logic, Schedule, and Method Calls) can enable or disable alarms independently. As a result, a User, Logic program, Schedule, or Method Call can:

If Independent is disabled:

For more information, see How the Independent Feature Works.

To enable or disable the Independent feature, you need to use the Server Configuration Tool. The Independent check box is in the Disable Alarms section of the Alarms settings:

To enable Independent so that Geo SCADA Expert considers the ‘Disable Alarms’ flag of each User Type before enabling alarms:

To disable Independent so that Geo SCADA Expert applies Disable Alarms or Enable Alarms whenever it is triggered:

Further Information

Enable Alarms: see Enable Alarms

Disable Alarms: see Disable Alarms


Disclaimer

Geo SCADA Expert 2020