Troubleshooting Statically Assigned Ports

For statically assigned ports, ViewX, Virtual ViewX and Original WebX clients can only display messages that relate to the TCP/IP network connection between the Geo SCADA Expert servers and the remote computer. Any errors relating to TCP/IP connection failures will be displayed as event messages in the Events List and as alarms on alarm displays such as the Alarm Banner, Lists, and suitably configured Mimics.

If there are communication problems on a statically assigned port, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2020