Working with the Geo SCADA Expert Server Configuration Tool

When you have started Geo SCADA Expert as a service, you may need to make some alterations to the Geo SCADA Expert server configuration. For example, you may need to change the Partners settings so that the Geo SCADA Expert server is used as part of a multi-server system rather than the default Lone Server arrangement.

To make alterations to the Geo SCADA Expert server configuration, you need to use the various features of the Geo SCADA Expert Server Configuration Tool.

Before you begin to configure the server(s), you should familiarize yourself with the Geo SCADA Expert Server Configuration Tool. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2020