Connected Workstations

The Workstation Name feature allows a single ViewX client PC (as opposed to a Virtual ViewX client PC) to be allocated a unique name called the Workstation ID. The Workstation ID is used to identify the client along with its IP address. It allows alarm responses to be restricted to a specific client PC (only users that log on to the client with the required Workstation ID can respond to the alarms).

You can use the Server Status Tool to view status information about the clients with Workstation IDs that are currently connected to the Main server or a Standby server. The status information is shown on the Connected Workstations section of the Server category.

If the Server Status Tool is connected to the Main server, the Connected Workstations status shows all clients that are connected to the system, including those connected to Standby servers. However, if the Server Status Tool is connected to a Standby server, the Connected Workstations status just displays information about the clients connected to that same Standby.

The Connected Workstations status information is categorized as:


Disclaimer

Geo SCADA Expert 2020