Lock Diagnostics Read

The Lock Diagnostics Read category provides summary information about database read lock usage. You can use this information when analyzing system performance.

For status information regarding locks in Geo SCADA Expert, see Locks. The Locks category displays all locks within the server, whereas database locks are specific to the 'database' and assist in identifying which operation is causing high lock utilization.

The database read locks are shown in rows, with each row representing a different lock. The status information shown for each lock is as follows:

You can access a context-sensitive menu by right-clicking on an entry in the list.

The options that are available are:

ATTENTION: These menu options apply to both database read and database write locks together. So, for example, the Reset Lock Diagnostics option will reset the write lock diagnostics and the read lock diagnostics.


Disclaimer

Geo SCADA Expert 2020