Full Install
When you select Full (Recommended) on the Choose Setup Type ‘page’ of the Geo SCADA Expert Installer, the following components will be installed:
- ViewX Client
- ViewX Help
- Aquis
- Crystal Reports*
- SCADAPack x70
- Server
- Server Side Help
- Configuration Samples
- Example Database
- Symbol Library
- Password Blacklist
- Example FloBoss configuration
- Example ROC Plus configuration
- Example Totalflow configuration
- Web Server
- DNP3
- SCADAPack E
- EtherNet/IP
- IEC 60870-5
- Kingfisher
- Modbus
- Advanced
- SCADAPack Modbus
- Modbus RTU Slave
- MQTT
- JSON Schema A
- NTP Monitor
- ODBC Client
- OPC Client - Advanced
- Pager
- Schneider Electric EcoStruxure Web Services Client - Advanced
- Schneider Electric SCADAPack 50
- Schneider Electric SCADAPack x70
- DNP3 Protocol
- SNMP Manager
- SQL Export
- Trio Diagnostics - Advanced
- Data Access
- Server Management Utilities
- WebX Client
(for Original WebX).
These components include the Geo SCADA Expert server, ViewX Client, WebX Client (for Original WebX), Data Access (for OPC, ODBC, OLEDB, Web and COM connections), and many of the available drivers. When installed, this will allow Geo SCADA Expert server and one ViewX client to run on the machine.
* The Crystal Reports client component is only included if the SAP Crystal Reports runtime components have been installed.
The SAP Crystal Reports runtime components are NOT installed by default. If you intend to install them you must purchase a Crystal Reports runtime license for each server on which these components are to be operational (clients do not need a license to use the runtime components). For servers on which the runtime components are operational, the Crystal Reports runtime license is included with the Geo SCADA Expert Crystal Reports driver license. Please contact your Schneider sales representative for more information.
If you intend using Crystal Reports on your system, you also need to install the Crystal Reports prerequisites and driver on any
If additional drivers are required, you will need to use the Custom install option (see Custom Setup).
The
When you choose the Full (Recommended) option, the Geo SCADA Expert Installer proceeds to the Super User Account ‘page’ automatically (see Create a Super User Account).