Welcome to the Schneider Electric Geo SCADA Expert Setup Wizard
The Welcome to the Schneider Electric Geo SCADA Expert Setup Wizard ‘page’ is the first ‘page’ of the installation wizard. It provides you with information about the version of Geo SCADA Expert you are about to install.
Virtual ViewX is supported by Geo SCADA Expert 2019 onwards. We strongly recommend that you install the Virtual ViewX server on a different machine to the Geo SCADA Expert server. This is to avoid potential performance issues due to the number of resources that each application uses.
If you do install Geo SCADA Expert and Virtual ViewX on the same machine, both applications must have the same version and build number. This is because the applications share some resources.
Select Next to proceed to the End-User License Agreement.