Configuring a TBox Outstation Set
An Outstation Set is a group of outstations that share the same channel(s). For further information on outstation sets, see Configuring an Outstation Set in the Geo SCADA Expert Guide to Advanced Drivers.
TBox supports the following types of outstation set:
- TBox Direct Outstation Set: a set of outstations using a single Direct Channel.
- TBox PSTN Outstation Set: a set of outstations using a single PSTN Channel.
- TBox Shared Outstation Set: a set of outstations sharing redundant direct connections from the Geo SCADA Expert server to the TBox device. Each outstation in the set can use either channel to communicate with the Geo SCADA Expert server.
- TBox Switched Outstation Set: a set of outstations sharing redundant direct connections from the Geo SCADA Expert server to the TBox device. All of the outstations in the set use the same channel at the same time, but the link can be switched to the second channel (for example, if the normal channel fails).
You need to be aware of the hardware setup on your system, as you need to configure the outstation sets that correspond to the type of communications used by the outstations in your system, and the channel(s) that those outstations use.
Before you configure an outstation set, configure the channels required by the outstations in the set (see Configuring a TBox Channel).
Configure the outstation set before you add the outstations to that set.
There are no driver-specific properties for TBox outstation sets. For information on configuring properties on the TBox Outstation Sets, see Configuring an Outstation Set in the Geo SCADA Expert Guide to Advanced Drivers.
Minimum Configuration
For a TBox Outstation Set to be capable of functioning, you need to specify the minimum settings for an outstation set: see Minimum Configuration in the Geo SCADA Expert Guide to Advanced Drivers.
.