Specify Whether to Update an Output Point Value Immediately Following a Control Action
This section applies only to TBox Analog Output Points and TBox Digital Output Points. For both of these point types, an Update point on successful action check box is displayed at the bottom of the Control tab.
Select the Update point on successful action check box for the point value to be reported immediately following a successful control action.
Clear the check box for the point value to be reported in the next poll.