Display the Default Time Scale on a Trend

You can reset a Trend so that it shows the time scale and value range that it displayed when you first accessed the Trend. This is useful when you have used the navigation tools and need to revert to the Trend’s original display.

To reset the Trend so that it displays its original time scale and value range:

  1. Right-click on the X-Axis.
    A context sensitive menu is displayed.
  2. Select the Revert to Defaults option.
    The Trend is reset so that it shows the same time scale and value range as it displayed when you first accessed the Trend.

Disclaimer

Geo SCADA Expert 2020