Created

Associated with: All items

This status attribute is only displayed for new items. It is replaced with the Last Modified attribute as soon as an item’s configuration is modified.

The Created attribute indicates the date and time at which an item was added to the database. The attribute also lists the name of the user that was logged onto the system from that node (workstation) at the time.

Example:

2007-06-14 12:29:13.891 by Engineer1
(Indicating that an item was added to the database at the time and date that is specified. ‘Engineer1’ was the user that was logged onto the workstation at that time.)


Disclaimer

Geo SCADA Expert 2020