Type

Associated with: All items

This status attribute comprises a standard description of the type of item.

Use the attribute in conjunction with the Full Name status attribute and, if applicable, the Source status attribute, to ascertain a particular item’s function and location on your system.

Example:

Modbus Digital Point
(Indicating that the item is the type of digital point that is supported by Geo SCADA Expert's Modbus driver. (The point represents digital data on a device with which Geo SCADA Expert communicates using the Modbus protocol, via Geo SCADA Expert's Modbus driver.))


Disclaimer

Geo SCADA Expert 2020