Using Auto Hide for a Tool Window

The Auto Hide feature allows you to hide a Tool Window, so that only the window's tabs are visible along the edge of the ViewX window.

This allows you to increase the space available for the document display area, while still providing easy access to the hidden tools if required.

Auto Hide is not available for a Document Window.

To enable the Auto Hide feature for a tool window:

Either:

Or:

Or:

The window appears as a set of tabs that run along the adjacent edge of the ViewX clientwindow.

To view a tool window that is currently hidden:

Perform one of the following:

To disable the Auto Hide feature for a tool window:

Perform one of the following:


Disclaimer

Geo SCADA Expert 2020