Configure the Y-Axis Color and Position
You can specify the color and position of the y-axis. You do this using fields in the Y-Axis Properties window (see Configure the Y-Axis Properties).
Use the Axis section of the window to specify these axis properties:
- Color: Use the Color button to specify the required color. You can select a color from the Color Palette or select the ... option to display the Color window. You can use the Color window to create a custom color (see Using the Color Window in the Geo SCADA Expert Guide to Core Configuration).
- Position: Use the combo box to specify the position of this axis on the display. The options vary, depending on the type of axis for which you are configuring the axis position. Choose 'Both' to display the axis at each of the positions offered.