Enable or Disable TCP/IP Functionality
            Use the Enabled check box at the top of the SCADAPack TCP/IP tab to specify whether TCP/IP functionality is enabled for the SCADAPack E outstation.
                
            
Select the Enabled check box for the other fields on the tab to become available.
Ensure that the check box is clear if the outstation does not require TCP/IP support.