Define the Set Clock Method

A SCADAPack controller's clock can be synchronized from Geo SCADA Expert or another source. To define which clock synchronization method you are applying, use the Set Clock Method field on the SCADAPack tab.


With a Realflo-enabled SCADAPack controller, the options are:

Ensure that any Advanced Modbus Outstation Sets that contain Realflo controllers have their Broadcast Set Clock feature disabled. (The Realflo method of setting a clock results in a Realflo controller restarting its current Hour log.)


Disclaimer

Geo SCADA Expert 2020