For a Flow Run that is Configured Directly in Geo SCADA Expert

Before you can successfully configure a Flow Run directly in Geo SCADA Expert:

As a minimum, for a Flow Run to be functional (online), you need to configure:

You then need to put the Flow Run In Service and save the configuration.

In order to produce a fully functional Flow Run, you will also need to use the Write Configuration pick action to write the configuration to the Realflo controller on which the Flow Run is located.


Disclaimer

Geo SCADA Expert 2020