Measurement Units
This section describes the units of measurement that are supported by Realflo. Select the tables in the sections that follow to view the measurement units for each type of parameter.
- US1 Units - are used for gas flow runs
- US2 Units - are used for gas flow runs
- US3 Units - are used for gas flow runs
- US4 Units - are used for gas flow runs
- US5 Units - are used for gas flow runs
- US6 Units - are used for gas flow runs
- US7 Units - are used for gas flow runs
- US8 Units - are used for gas flow runs
- PEMEX Units- are used for gas flow runs
- IP Units - are used for gas flow runs
- IP2 Units -are used for liquid and water flow runs
- IP3 Units - are used for liquid and water flow runs
- IP4 Units - are used for liquid and water flow runs
- IP5 Units - are used for liquid and water flow runs
- Metric 1 Units - are used for gas, liquid, and water flow runs
- Metric 2 Units - are used for gas, liquid, and water flow runs
- Metric 3 Units - are used for gas, liquid, and water flow runs
- Metric 4 Units - are used for gas, liquid, and water flow runs
- SI Units - are used for gas flow runs.