When in Full Screen mode, it is still possible to close or hide all of the menus, Explorer bars, status bar etc. If you are unfamiliar with the ClearSCADA keyboard shortcuts, this may cause you a problem as without them, you won't be able to access the database objects and menu options that you need to use.
To re-display the menu options and Explorer bars, you need to use keyboard shortcuts. In Full Screen mode, you may find the following keyboard shortcuts useful:
Keyboard Shortcut | Function |
---|---|
F11 | Toggle Full Screen Mode |
Ctrl + B | Toggle Alarm Banner |
F9 | Display All Alarms List |
F10 | Display All Events List |
Ctrl + D | Display Database Explorer Bar |
Ctrl + E | Display Document Store Bar |
Ctrl + I | Display Favorites Bar |
Ctrl + T | Display OPC Data Bar |
Ctrl + R | Display OPC Historic Bar |
Ctrl + Q | Display Queries Bar |
Ctrl + W | Display Windows selection dialog (allows you to choose which display is currently active) |
Alt + Home | Display the Home page for the currently logged on user. |