ClearSCADA provides a range of interfaces to allow connection with third party products. The interfaces include:
- ODBC
- OPC DA
- OPC HDA
- OPC AE
- OPC XML-DA
- Automation Interface
- .Net API
- SOAP / XML
- Communications drivers
- Communication slaves (where ClearSCADA emulates a PLC/RTU)
This section provides specific information about different software packages and the ways in which they can be interfaced with ClearSCADA. Any known issues or limitations on the interface will be noted along with detailed instructions on how to setup the connection.
Page:
Application Encryption
Page: Configuring a Linked ODBC Table to MySQL
Page: Connect from SQLServer 2005 using Linked Servers
Page: Connecting to Autosol OPC Server
Page: Connect to ClearSCADA Using OPC - OPC Protocol Details
Page: How to create the LinkedODBCTable from ClearSCADA Server Configuration to connect to MS SQL Server
Page: OPC Quality Flags
Page: Supported Interface and Protocol Versions
Page: Configuring a Linked ODBC Table to MySQL
Page: Connect from SQLServer 2005 using Linked Servers
Page: Connecting to Autosol OPC Server
Page: Connect to ClearSCADA Using OPC - OPC Protocol Details
Page: How to create the LinkedODBCTable from ClearSCADA Server Configuration to connect to MS SQL Server
Page: OPC Quality Flags
Page: Supported Interface and Protocol Versions