Geo SCADA Expert

This page provides information on compatibility between different versions of ClearSCADA, Windows Operating Systems and Internet Explorer software. Use this information during the upgrade process to determine whether your current installation environment is compatible with newer versions of ClearSCADA.

Supported
Not Supported
ClearSCADA Server Support Only
See Note

In all cases, you should follow the upgrade instructions for the version to which you are upgrading.

  ClearSCADA 2015 R1
ClearSCADA 2015 R2
ClearSCADA 2017 ClearSCADA 2017 R2 ClearSCADA 2017 R3 Geo SCADA 2019 Geo SCADA 2020
Windows Server 2019 - 64 bit






Windows Server 2016 - 64-bit






Windows 10 - 64 bit





(Note 3)
Windows 10 - 32 bit

(Note 2)

(Note 2)

(Note 2)

(Note 2)

(Note 2)

(Note 2) (Note 3)
Windows 8.1 - 64 bit



Windows 8.1 - 32 bit
(Note 2)

(Note 2)

(Note 2)

(Note 2)

(Note 2)


(Note 2)
(Note 2)
Windows Server 2012 R2 - 64 bit




Windows 8 - 64 bit



Windows 8 - 32 bit
(Note 2)

(Note 2)

 (Note 2)

(Note 2)

(Note 2)

(Note 2)
Windows Server 2012 - 64 bit


Windows 7 - 64 bit
Windows 7 - 32 bit
(Note 2)

(Note 2)

 (Note 2)

(Note 2)

(Note 2)

(Note 2)
Windows Server 2008 R2 - 64 bit
Windows Server 2008 - 64 bit
Windows Server 2008 - 32 bit
Windows Vista - 64 bit
Windows Vista - 32 bit
Windows Server 2003 R2 - 64 bit
Windows Server 2003 R2 - 32 bit
Windows Server 2003 - 64 bit
Windows Server 2003 - 32 bit
Windows XP - 32 bit
           


ClearSCADA Server Support Only
The new ViewX Client application included with ClearSCADA 2014 R1.X does not support Windows Server 2003 or Windows Server 2003 R2 and will not be functional. Only the ClearSCADA Server will be functional when installation is performed on these operating systems.
NOTE 1 - KepServerEX PLC Driver
Please note that the PLC Driver in ClearSCADA (KEPServerEX) is not compatible with Windows 7, Windows Vista, Windows Server 2008 or Windows Server 2012 operating systems. The driver may not run properly if installed on these operating systems. The KEPServerEX PLC Driver is not included with versions of ClearSCADA after 2013 R2.
NOTE 2 - Server Components - Limited 32-bit OS Support
64-bit OS versions are recommended as 32-bit OS has limited server component support.
Starting in ClearSCADA 2015 R1, ClearSCADA Mobile and new WebX (deployed through IIS) require a 64-bit OS to install the necessary server components.
Starting in Geo SCADA 2019, Virtual ViewX server (deployed through IIS) require a 64-bit OS to install the necessary server components and the server is not supported on Windows Server 2008, Windows 7 or Windows 8.
NOTE 3 - Windows 10 Version
Geo SCADA 2020 will support Windows 10 Versions from 1809 upwards.