Geo SCADA Expert

When installing additional ClearSCADA features, some components may be installed while the ClearSCADA server in still running. These components include drivers and other system utilities such as the Alarm and Event Printer.

If a new driver is installed while the system is running, it will not be available to run on the server or to create objects on the clients until the server is restarted. On restart, the new driver will be recognized and started as expected.