Geo SCADA Expert

Description:

In ClearSCADA Server Configuration, the user enter in Global Parameters → Performance Monitor,  System Configuration → Printing, and System Configuration → System Calls required that this Windows User must have "Log on as a service" privilege and or "Replace a process level token" privilege. 

In order to add these Windows privileges, please do the followings:

1.   Windows Start Button --> Run and type in "gpedit.msc"

2a. In Windows XP open the following path:
 
 
2b.  In Windows 7, Windows 2008, open the following path: