Label: cybersecurity

Content with label cybersecurity in Geo SCADA Expert Software (See content from all spaces)
Related Labels: secure, encryption, ssl

Page: Application Encryption
Encryption Overview Encryption is one of many possible solutions to assist to protect your system against attackers. In the case of ClearSCADA encryption is used specifically to improve the confidentiality and integrity of the system by encrypting the connection between servers, and between server and client, as well ...
Page: Disabling the SSL server Null cipher
Problem ClearSCADA uses a SSL server that supports a number of ciphers including the Null cipher (TLSRSAWITHNULLSHA and TLSRSAWITHNULLMD5). The Null ciphers are a 0bit SSL cipher which do not provide encryption for any connection using the cipher and, depending on the environment, could be the negotiated ...
Other labels: ssl, encryption, secure