Label: logic

Content with label logic in Geo SCADA Expert Software (See content from all spaces)
Related Labels: performance, linked, sql, tables, clearscada

Page: Accessing Data via SQL in Structured Text
structured text program you can define simple variables using %M, %I and %Q, however useful these are they are static. There is a more dynamic way of reading data from ClearSCADA to use in a structured text program that returns the data in the form of a "resultset ...
Other labels: clearscada, sql
Page: Logic Execution
logic engine is single threaded, this means that ClearSCADA can only run one logic program at a time. To protect logic programs from being affected by poorly written logic programs that cannot execute correctly ClearSCADA includes an instruction ...
Other labels: clearscada, linked, tables, sql, performance