Label: opc

Content with label opc in Geo SCADA Expert Software (See content from all spaces)
Related Labels: version, odbc, clearscada, dcom, interface

Page: OPC and DCOM
OPC is based on Microsoft's Component Object Model (COM). When you are using OPC connections across multiple machines, then DCOM (distributed COM) comes into play. Configuring DCOM is an issue which often causes a lot of grief and this section ...
Other labels: dcom, clearscada
Page: Supported Interface and Protocol Versions
Geo SCADA Expert / ClearSCADA supports a number of interfaces and protocols for transporting data into and out of the database depending on the needs of the user and the requirements of the software involved. The following tables lists the interfaces available and the versions supported. Where the  Version Support is blank ...
Other labels: interface, version, odbc