ClearSCADA provides a command line utility that allows users to start and stop the server, as well as perform a number of other management tasks. This utility, named scxcmd.exe, can be found in the program installation directory.
{code:html}
ClearSCADA Command Line Utility
Usage: scxcmd \[options] command
{code}
{tip}For a full and up to date list of options available, run scxcmd \-?.{tip}
h3. scxcmd Options
|| Option || Description ||
| \-s server\[:port\] | Connect to specified server and port. Defaults to localhost:5481 |
| \-u user | Log on with specified user name |
| \-p password | Log on with specified password |
| \-h, \-? | Display the help for scxcmd |
h3. Commands
|| Command || Description ||
| START DB | Start or repair the database if necessary (i.e. when in Invalid Configuration state). |
| START driver | Start the specified driver. |
| START DRIVERS | Start all drivers. |
| STOP SERVER | Stop the server. |
| STOP driver | Stop the specified driver. |
| STOP DRIVERS | Stop all drivers |
| RESTART driver | Restart the specified driver. |
| RESTART DRIVERS | Restart all drivers. |
| COMPRESSDB | Compress the database. |
| SETLOG \{DB \| driver\} options | Set the logging options for the database or specified driver |
| ADDLOG \{DB \| driver\} options | Add logging options to the database or specified driver |
| REMLOG \{DB \| driver\} options | Remove logging options from the database or specified driver |
| SHOWLOG \{DB \| driver\} options | Show logging options for the database or specified driver. |
| SHOWDIAG diag | Show the specified diagnostic page. Use SHOWDIAG HELP to display a list of available diagnostics. |
| SHOWSTATE | Show the current server state |