compared with
Key
This line was removed.
This word was removed. This word was added.
This line was added.

Changes (28)

View Page History
h3. scxcmd Options

||Option||Description|| || Option || Description ||
|-s server\[:port]|Connect | \-s server\[:port\] | Connect to specified server and port. Defaults to localhost:5481 |
|-u user|Log | \-u user | Log on with specified user name |
|-p password|Log | \-p password | Log on with specified password |
|-h, -?|Display | \-h, \-? | Display the help for scxcmd |

h3. Commands

||Command||Descriptio|| || Command || Description ||
|START DB|Start | START DB | Start or repair the database if necessary (i.e. when in Invalid Configuration state). |
|START driver|Start | START driver | Start the specified driver. |
|START DRIVERS|Start | START DRIVERS | Start all drivers. |
|STOP SERVER|Stop | STOP SERVER | Stop the server. |
|STOP driver|Stop | STOP driver | Stop the specified driver. |
|STOP DRIVERS|Stop | STOP DRIVERS | Stop all drivers |
|RESTART driver|Restart | RESTART driver | Restart the specified driver. |
|RESTART DRIVERS|Restart | RESTART DRIVERS | Restart all drivers. |
|COMPRESSDB|Compress | COMPRESSDB | Compress the database. |
| SETLOG \{DB \| driver\} options | Set the logging options for the database or specified driver |
| ADDLOG \{DB \| driver\} options | Add logging options to the database or specified driver |
| REMLOG \{DB \| driver\} options | Remove logging options from the database or specified driver |
| SHOWLOG \{DB \| driver\} options | Show logging options for the database or specified driver. |
|SHOWDIAG diag|Show | SHOWDIAG diag | Show the specified diagnostic page. Use SHOWDIAG HELP to display a list of available diagnostics. |
|SHOWSTATE|Show | SHOWSTATE | Show the current server state |
|HISDUMP filename|Dump | HISDUMP filename | Dump contents of historic file |
|HISFLUSH|Perform | HISFLUSH | Perform historic flush. |
| HISGEN | Generates Historic Data for performance etsting. |
| HISINFO filename \[Recurse]|Counts \[Recurse\] | Counts duplicates and deleted records in a historic file. |
| HISSTRIP filename \[Recurse]|Removes \[Recurse\] | Removes duplicates and deleted records from historic file. |
|SETSYSTIME DB|Set | SETSYSTIME DB | Set server clock to specified SystemTime |
|GETSYSTIME DB|Get | GETSYSTIME DB | Get server clock as SystemTime |