Geo SCADA Expert

This site's content is being moved
View the Geo SCADA Expert content in Schneider Electric Exchange
Please bear with us as we tidy and improve the pages. We welcome comments on the Geo SCADA Expert Forum

compared with
Current by Steve Beadle
on Feb 24, 2020 07:32.

Key
This line was removed.
This word was removed. This word was added.
This line was added.

Changes (1)

View Page History
Using the automation interface with C# is very similar to using it within VB, apart from the obvious syntax differences between the two languages.

We do recommend you use the .Net Client interface though. {color:#000000}If you look in the Start Menu folder for ClearSCADA, you'll notice a "Client API" shortcut. This link will take you to the documentation for the automation interface. You should start in the ClearScada.Client.Simple Namespace. The key classes to use are "Connection" and "DBObject".{color}

However, to use the automation interface:
# When C# is running, select Project - Add Reference
# Select the COM tab