<Dynacard Type> Dynacard

Associated with: Dynacard Stores

The name of this status attribute indicates the type of dynacard for which a set of data is stored online (for example, ‘Last Stroke Dynacard’). The status attribute displays the date and time at which ClearSCADA uploaded the set of dynacard data to the Dynacard Store.

For those types of dynacard for which ClearSCADA can retain multiple sets of data online, the name of the status attribute is prefixed with a number. The number indicates the particular set of dynacard data to which the set of status attributes relate. (Settings on the Dynacard Store’s configuration Form determine how many sets of certain types of dynacard data a Dynacard Store retains online (see Configure the Dynacard Storage Properties).)

For those types of dynacard for which the Dynacard Store can only retain one set of data online, the status attribute displays the value Not Present if ClearSCADA has never uploaded that type of dynacard data to the Dynacard Store.

Example:

3 Stored Dynacard: 21/Jun/2012 16:09:56.031

(The ‘3’ indicates that this status attribute relates to the third set of ‘Stored’-type dynacard data associated with this particular Dynacard Store. ClearSCADA uploaded the set of data at 16:09:56.031 on 21st June 2012.)

Use the status attribute in conjunction with the relevant Number of Points and Outstation Timestamp status attributes.


Disclaimer

ClearSCADA 2017 R2