Outstation Timestamp

Associated with: Dynacard Stores

This status attribute indicates the date and time at which the outstation retrieved the set of dynacard data from the well’s sensors.

Use the status attribute in conjunction with the relevant <Dynacard Type> Dynacard and Number of Points status attributes.


Disclaimer

ClearSCADA 2017 R2