Ascertain Which Alarm Redirections are Pending or in Progress

You can use the Alarm Redirections section of the ClearSCADA Server Status Tool to ascertain which alarm redirections are pending or in progress on your ClearSCADA system (see Alarm Redirections in the ClearSCADA Guide to the Server Status Tool).

The section shows those alarm redirections that are to be triggered automatically (see Define the Trigger Type). Manual alarm redirections are executed as soon as they are requested, and therefore do not appear in this section.


Disclaimer

ClearSCADA 2017 R2