Client-Specific Alarms List and Alarm Banner Preferences

This section summarizes those Alarms List and Alarm Banner options that a system administrator can configure on a per client basis. Such options, if required to differ from the defaults, should be specified on existing ClearSCADA Clients (workstations) when a ClearSCADA system is first installed, and then on new clients whenever they are added to the system. On each ViewX Client, you specify the options using the Options window.

You can use the Options window to specify:

For anyone who accesses the system without logging on via a User Account, use the Options window to define the client-specific Features that are available to the Guest User, including:

For information on configuring either of the above, see Define the Client Specific Settings for the Guest User in the ClearSCADA Guide to Security.

In addition to the above, whenever a ViewX client is added to the system, a system administrator has to specify the connection between that client and the system. This is done using the Client Configuration window. The window is also used to specify:

Further Information

Display the Alarm Banner in Full mode on a Multi-Monitor Setup: see Launch the Alarm Banner in Full Mode in the ClearSCADA Guide to Client Administration.


Disclaimer

ClearSCADA 2017 R2