Configure a Firewall for a WebX or XML Client - System Connection

If your system uses a firewall between the WebX or XML client and the ClearSCADA server, you need to configure it so that it allows communications via the port used by the web server. If the default settings are in place, this means that the firewall has to allow ports 80 and 443. If the default ports are not used, you will need to configure the firewall to allow the ports used by your system.

You can see which ports are being used by the web server on your system by examining the following:

For more information about firewalls, please refer to the manufacturer’s documentation supplied with your firewall.


Disclaimer

ClearSCADA 2017 R2