Edit an Existing ViewX Client - Third Party OPC Server Connection
You can use the ClearSCADA Client Applet to change the configuration of an existing ViewX client - Third Party OPC server connection. This is useful when you need to alter the way the client - OPC server connection works, for example, you may need to rectify a mistake such as having selected the wrong Type of OPC server.
To edit an existing ViewX client - Third Party OPC server connection:
- On the ViewX client, use the Windows Start menu to access ClearSCADA’s Configure Connections option and run the ClearSCADA Client applet.
- Select the ViewX - Third Party OPC server connection that you want to edit.
- Select the Edit button to display the ClearSCADA Client Configuration window.
- Use the ClearSCADA Client Configuration window to change the System Name, Type, Visible in ViewX and Node settings as required. For more information on these settings, Create a Connection between a ViewX Client and a Third Party OPC Server.