Defining the Format of Displayed Values

Point values are shown on a variety of displays within ClearSCADA. You can:

Engineers with programming experience can also use the expression function FORMATVAL to define the format of a value in ClearSCADA (for example, in a Mimic animation). You can include any of the following syntax in the ‘Format String’ argument of the FORMATVAL function: Date and Time Syntax, Numeric Syntax, Text String Syntax, and Boolean Syntax.


Disclaimer

ClearSCADA 2017 R2