Specify the Data that ClearSCADA Stores for an Accumulator

Use the Historic Data Filter section of the Reset tab in conjunction with the Historic tab.

The Historic tab defines whether the server stores Accumulator values historically, and whether any unnecessary data is filtered out to reduce storage requirements (see Tabs on Accumulator Forms).

Use the fields within the Historic Data Filter section of the Reset tab to specify the type of Accumulator data that ClearSCADA is to store historically:

If none of the check boxes is selected, regardless of whether historic is enabled on the Historic tab, ClearSCADA will not store retrieved Accumulator values historically.


Disclaimer

ClearSCADA 2017 R2