The Format in which Schedule Times are Displayed
The format in which a schedule’s trigger times are displayed in the Schedule Times window varies, depending on the type of Schedule and whether that Schedule is associated with a Calendar.
The same format is also used in the Add Time and Edit Time windows that are displayed when you add or adjust an event time using the Schedule Times window (see Add an Event using the Schedule Times Window, and see Move an Event).
This section explains, via a series of examples, the formats in which event times are displayed.
Example: