Add an Event using the Schedule Times Window

This section applies to Schedules other than Simple Schedules.

You generally add event(s) to a Schedule by adding those events directly to the Schedule Display (see Add an Event Directly to a Schedule). However, you can also add events to a Schedule by using the Add button on the Schedule Times window.

To add an event to a Schedule by using the Schedule Times window:

  1. Display the Schedule Times Window.

    (The Format in which Schedule Times are Displayed varies, depending on the type of Schedule.)

  2. Select the Add button.
    The Add Time window is displayed, with the first element of the time or date highlighted.

  3. If the entry includes a day, month, or Calendar day type, use the Up and Down arrow keys on your keyboard to cycle through the available options and select the required entry.
  4. Select the first time element (for instance the hour) and either overwrite the time with the required time, or use the field’s arrows to select the required time.
  5. Repeat step 4 for any other time element(s) (such as minutes).
  6. Select the OK button to add the new time to the Schedule Times window.
  7. Repeat steps 2 to 6 for any other times that you want to add to the window.
  8. Select the OK button on the Schedule Times window to add the event times to the Schedule.
  9. Save the configuration.

Disclaimer

ClearSCADA 2017 R2