Define Whether an Initialization Request Requires Confirmation

Many counter-type points support initialization, whereby an operator can initialize the point back to a particular value by using the Initialize or Enable / Disable pick action.

The Confirm Initialize (Confirm Disable/Enable) combo box is displayed on the Point Form for counter-type points that support Initialization. (On some drivers, the name of this combo box varies—see the driver-specific documentation for details.)

Use the Confirm Initialize combo box to define whether a confirmation dialog box is displayed whenever an operator requests that a point is initialized (see Requesting Confirmation of Action Requests in the ClearSCADA Guide to Core Configuration).


Disclaimer

ClearSCADA 2017 R2