Configuring String Points

Use DDE String points to map text strings on DDE servers into ClearSCADA.

Configure the properties of each String point using the fields on the DDE String Point Form.

For information on the String Point tab on the String Point Form, see Defining String Point Details in the ClearSCADA Guide to Core Point Configuration.

For information on the fields on the DDE tab, see Configure Common Properties on the DDE Tab.

For information on the Control tab on the Form, see Define the Control Settings for a String Point in the ClearSCADA Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.


Disclaimer

ClearSCADA 2017 R2