Working with the Database Schema
The ClearSCADA Database Schema is a web based display that provides information about the various classes in the database. Each class has its own page that contains details about:
- Base Class—The class that is immediately above the selected class in the database hierarchy.
- Sub-Classes—The classes that are immediately below the selected class in the database hierarchy.
It also provides details about the various fields, aggregates, and methods that are contained within the class.
This section explains how to use the ClearSCADA Database Schema and describes some of the potential entries.
To familiarize yourself with the ClearSCADA Database Schema, you should: