Configure the General Point Properties

Use the fields at the top of the Digital Point tab to define the general properties of an IEC 60870-5 Digital Point (see Configure Common IEC 60870-5 Point Properties). Fields that are specific to IEC 60870-5 Digital Points are summarized below.


Disclaimer

ClearSCADA 2017 R2