System Analysis

This section is designed for use by system administrators and high-level engineers when assessing the state of the ClearSCADA system. It describes the statistical and diagnostic information provided specifically for the IEC 60870-5 driver. For more general information on analyzing a ClearSCADA system, see System Analysis in the ClearSCADA Guide to the Server Status Tool.

During system analysis, you might need to:

Additionally, if an outstation is not communicating with the server when it should be, see Troubleshooting in the ClearSCADA Guide to Advanced Drivers.

When troubleshooting on a ClearSCADA system, examine the diagnostic messages in the Events List. The messages may help you to identify the cause of any problems.

Further Information

Understand and Resolve Outstation Interrogation Alarms.


Disclaimer

ClearSCADA 2017 R2