ADD_DT_TIME
Function Name |
ADD_DT_TIME |
---|---|
Description |
Adds a date and time input to a time interval input and outputs the result. |
Arguments |
Input 1 {DATE_AND_TIME} Input 2 {TIME} For more information on the data types for the inputs and outputs, see Data Type Hierarchy. |
Returns |
Output {DATE_AND_TIME} |
Example:
Function Block Diagram - ADD_DT_TIME:
An ADD_DT_TIME function has two inputs:
- Input 1 is a date and time value (in this case, a NOW function which provides the current date and time)
- Input 2 is a constant with a time value of T#10m (10 minutes).
You can use the UTC_TO_LOCAL function to convert the NOW input from UTC time to Local time.
The ADD_DT_TIME function adds the time interval defined by Input 2 (10 minutes) to the NOW time, and outputs the result. So, if the NOW time is 2006-03-21-09:27.31.546, the ADD_DT_TIME function adds 10 minutes to that time and outputs 2006-03-21-09:37.31.546.
ST Program - ADD_DT_TIME:
The syntax for an ADD_DT_TIME function in an ST Program is:
Output := ADD_DT_TIME (Input 1, Input 2)
Where Output, Input 1 and Input 2 are defined as variables earlier in the ST program. Each input is separated by a comma. Output and Input 1 are Date and Time values and Input 2 is a Time value (it defines an interval).
Further Information
Time Zones: see Time Zone Support in ClearSCADA in the ClearSCADA Guide to Core Configuration.