Define the Execution Method for a Logic Program

Each Logic program has an Execution Method setting that you can use to define whether the program is executed as a response to its inputs or on a timed basis.

The Execution Method setting provides two options:

To change the Execution Method of a Logic program, display the Logic Program Form, select the Logic tab, then choose the appropriate setting from the Execution Method combo box.

Further Information

Display the Logic Program Form: see Configure an ST Program, Ladder Diagram, SFC or FBD.


Disclaimer

ClearSCADA 2017 R2