Edit an ST Program

To enter the code for an ST program, you need to edit as ST Program database item. During the editing process, you will enter the code that defines the behavior that is to be provided by the program, for example, you could enter the code that allows the ST program to perform a calculation. When you save the code, the program you have created is stored in the ST Program database item.

To edit an ST program:

The main display area of the ST program editor shows the ST program. Each ST program has

PROGRAM <program name>

;

END_PROGRAM

by default as ST programs require these. You will define the Logic of your ST program between PROGRAM and END_PROGRAM.

At the bottom of the ST program editor is a smaller frame. This frame is the compiler. \ClearSCADA displays diagnostic information in this section.

To code an ST program, you need to understand the Structured Text language. We explain some of the basic principles of the ST language in these sections, but you may need to broaden your knowledge by referring to a Third Party source.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

The following sections explain how to check that your ST program is coded correctly:

The following section explains how to configure your ST program (including how to define when the program is executed):


Disclaimer

ClearSCADA 2017 R2