Function Block Diagrams

Function Block Diagrams are graphical programs that allow you to define a series of processes that are dependent on a flow. The flow of a signal from one function block to another means that you can create complex relationships between values, functions etc. to define the Logic behavior of your program.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

For information on the properties of the Function Block Diagram database items, see Logic Program Properties and Values.


Disclaimer

ClearSCADA 2017 R2