Border Tab

You can use the Border tab to define the appearance of the outline of a text box on a Mimic. The Border tab is only shown on the Text Properties window (see Editing a Text Box).

By using the settings on the Border tab, you can define the visibility, width, color, and flashing effects for the outline of a text box. The Arrow Heads settings are designed for lines and so are unsuitable for use with borders (as the border is a rectangle, with no ‘start’ and ‘end’).

The settings are:


Disclaimer

ClearSCADA 2017 R2