Change the Order of Custom Pick Actions, Menus, and Separator Lines

You can change the order of pick actions, pick action menus, and separator lines. To do this, you need to use the Move Up and Move Down buttons on the Pick Menu window.

To change the order of custom pick actions, custom pick action menus, and separator lines:

  1. Display the Pick Menu window (see Using the Pick Menu Window).
  2. Select the pick action, menu, or separator line that you want to move.
  3. Either:
    • Select the Move Up button to move the action, menu, or line toward the top of the hierarchy.
    • Select the Move Down button to move the action, menu, or line toward the bottom of the hierarchy.
  4. Repeat step 3 as required.

Disclaimer

ClearSCADA 2017 R2